17.2.11.1.2 set_device
(Ask a Question)Description
Specify family name, die name, and speed grade.
set_device -family <family_name> -die <die_name> -speed <speed>Arguments
| Parameter | Type | Description |
|---|---|---|
| -family <family_name> | String | Specify the family name. Possible values are PolarFire, PolarFire SoC, IGLOO 2, SmartFusion 2, and RTG4. |
| -die <die_name> | String | Specify the die name. |
| -speed <speed> | String | Specify the device speed grade. Possible values are STD or -1. |
| Return Type | Description |
|---|---|
| 0 | Command succeeded. |
| 1 | Command failed. There is an error. You can observe the error message in the console. |
List of Errors
| Error Code | Error Message | Description |
|---|---|---|
ERR0023 | Required parameter—die is missing | The die option is mandatory and must be specified. |
ERR0005 | Unknown die 'MPF30' | The value of -die option is not correct. See the possible list of values in option's description. |
ERR0023 | Parameter—die is missing value | The die option is specified without value. |
ERR0023 | Required parameter—family is missing | The family option is mandatory and must be specified. |
ERR0004 | Unknown family 'PolarFire®' | The family option is not correct. See the possible list of values in option's description. |
ERR0023 | Parameter—family is missing value | The family option is specified without value. |
ERR0023 | Required parameter—speed is missing | The speed option is mandatory and must be specified. |
ERR0007 | Unknown speed '<speed>' | The speed option is not correct. See the possible list of values in option's description. |
ERR0023 | Parameter—speed is missing value | The speed option is specified without value. |
Supported Families
| PolarFire® |
| PolarFire SoC |
| RTG4™ |
| SmartFusion® 2 |
| IGLOO® 2 |
Example
set_device -family {PolarFire} -die {MPF300T_ES} -speed -1set_device -family SmartFusion 2 -die M2S090T -speed -1