Description
Instantiate component SDC/PDC/NDC files into the design-level database.
derive_constraints
Arguments
| Return Type | Description |
|---|
| 0 | Command succeeded. |
| 1 | Command failed. There is an error. You can observe the error message in the console. |
List of Errors
| Error Code | Error Message | Description |
|---|
ERR0013 | Top-level is not defined | This means that the top-level module or entity is not specified. To fix this call, issue the set_top_level command before the derive_constraints command. |
Supported Families
| PolarFire® |
| PolarFire SoC |
| RTG4™ |
| SmartFusion® 2 |
| IGLOO® 2 |
Example
derive_constraints