15.4.1 Manufacturing Flows
(Ask a Question)The following sections discuss the different types of manufacturing flows.
15.4.1.1 HSM-based Manufacturing Flow
(Ask a Question)The HSM-based manufacturing process uses device-supported security protocols. For more information, refer to the Secure Production Programming Solution (SPPS) User Guide .
The U-HSM allows the user to generate and use various encryption and pass keys. Cryptographical operations requiring those keys are executed inside the security boundaries of the HSM Module:
Operation support for the HSM-based Manufacturing Flow is as follows:
- Key import, generation, and use under protection of the U-HSM and the M-HSM
 - Initial secure key injection into the device using the Authorization Code protocol
 - Secure data transmission between the U-HSM and the M-HSM
 - Overbuild protection
 - Device authentication
 - U-HSM verification of cryptographically sealed certificate of conformance (CoC) from the design programmed into the device
 - U-HSM verification programming job end certificates
 - Initiator and Upgrade programming job types
 - eNVM and sNVM client update
 - eNVM client selection
 - Security overwrite
 - Secure debug with SmartDebug tool
 
15.4.1.1.1 HSM Server Requirements
(Ask a Question)In the HSM-based Manufacturing Flow, the Job Manager is configured to work with the U-HSM to generate the HSM Programming Job, and HSM Programming Jobs require the M-HSM for job execution. For more information about HSM servers, refer to the Secure Production Programming Solution (SPPS) User Guide . For information about installation, refer to the User HSM Installation and Setup User Guide for the U-HSM and the Manufacturer HSM Installation and Setup User Guide for the M-HSM.
15.4.1.2 Non-HSM Manufacturing Flow
(Ask a Question)Non-HSM Manufacturing Flow support by the Job Manager allows bitstream file and programming job generation outside of the Libero tool. The Job Manager supports the following operations for non-HSM Manufacturing Flow:
- Initial key loading via KLK-protected bitstreams
 - Generate UEK1/UEK2/UEK3 encrypted update bitstreams
 - eNVM and sNVM client Update
 - eNVM client selection
 - Key value overwrite
 - Security overwrite