4.3.1 Installing a Floating License on a Windows Server
(Ask a Question)- 
                Download the licensing daemons from the Microchip Libero page.
                
- Go to the Download Software section.
 - 
                        Select the Daemons tab, and then select the
                            Windows Daemons file you want to download.
                        Tip: For convenience, select this link to download the Windows Daemon files.
 
 - 
                Create a folder named FlexLM in a root directory. For example:
                        
C:\FlexLM. - 
                Save the 
License.datfile in the folder you created in the previous step. - 
                Save the downloaded daemon to 
<directory_location>. - 
                Perform the following steps to edit the 
License.datfile:- 
                        Update the SERVER line by replacing
                                
<put.hostname.here>with the actual hostname without the angle brackets. - Modify the port number if necessary. The default port number is 1702.
 - 
                        Update the VENDOR and
                                DAEMON lines with the appropriate paths. For
                            example, see the following paths.
                                
DAEMON actlmgrd C:\flexlm\actlmgrd DAEMON saltd C:\flexlm\saltd VENDOR snpslmd C:\flexlm\snpslmd 
 - 
                        Update the SERVER line by replacing
                                
 - After making the necessary changes, save the file.
 - 
                To start the License Manager, type the following command from the command prompt:
                        
C:\flexlm\lmgrd -c C:\flexlm\License.dat - 
                To log the License Manager output, type the following command from the command prompt:
                        
C:\flexlm\lmgrd -c <path_to_License.dat>/License.dat -l /license.log