TCPIP_IPV4_PacketOptionGet Function
C
int TCPIP_IPV4_PacketOptionGet(
TCPIP_MAC_PACKET* pRxPkt,
TCPIP_IPV4_OPTION_TYPE optType,
IPV4_OPTION_FIELD* pOptField,
int optSize
);
Description
This function is a helper to allow retrieving a specific option that is present in an IPv4 received packet.
Preconditions
IPv4 properly initialized. pRxPkt a proper IPv4 packet received by the IPv4 module.
Parameters
Parameters | Description |
---|---|
pRxPkt | A packet received by the IPv4 module. |
optType | Type of options to be searched/retrieved. |
pOptField | Address to store the option. Could be NULL if not needed. |
optSize | Size of the pOptField structure, including the optData part. If 0, pOptField will not be updated. |
Returns
- Size of the option, if found in the IPv4 packet.
- 0 if such an option does not exist.
Remarks
The packet should be a proper IPv4 packet received through the IPv4 module. Only minimal consistency check is done.