TCPIP_IPV4_PacketTransmit Function
C
bool TCPIP_IPV4_PacketTransmit(
IPV4_PACKET* pPkt
);
Description
The IPv4 packet is sent to the MAC for transmission.
Preconditions
pPkt should have been properly formatted with TCPIP_IPV4_PacketFormatTx(). The packet interface should be updated.
Parameters
Parameters | Description |
---|---|
pPkt | The packet to be transmitted. |
Returns
- True - If the packet was handed to the MAC or is queued for transmission.
- False - The packet cannot be transmitted (wrong interface, etc.).
Remarks
Only single packets can be transmitted. Chained packets are not supported for now.