TCPIP_IPV4_MaxDatagramDataSizeGet Function
C
int TCPIP_IPV4_MaxDatagramDataSizeGet(
TCPIP_NET_HANDLE netH
);
Description
This function is a helper to allow retrieving the MDDS on the specified interface.
Preconditions
IPv4 properly initialized. Interface properly initialized.
Parameters
Parameters | Description |
---|---|
netH | Handle of the interface. |
Returns
- The maximum datagram data size that can be transported on the selected interface.
- 0 - Invalid interface specified.
Remarks
None.