TCPIP_IPV4_PacketOptionListGet Function
C
int TCPIP_IPV4_PacketOptionListGet(
TCPIP_MAC_PACKET* pRxPkt,
TCPIP_IPV4_OPTION_DCPT* pOptions,
int nOptions
);
Description
This function is a helper to allow retrieving a list of options that are present in the received packet.
Preconditions
IPv4 properly initialized. pRxPkt a proper IPv4 packet received by the IPv4 module.
Parameters
Parameters | Description |
---|---|
pRxPkt | A packet received by the IPv4 module. |
pOptions | Pointer to an array of option descriptors to receive the options present in the packet. |
nOptions | Number of elements the array can store. Could be 0, in which case pOptions is not updated. |
Returns
- The number of options found in the packet.
- 0 - Invalid packet or packet without options.
Remarks
The packet should be a proper IPv4 packet received through the IPv4 module. Only minimal consistency check is done. On return, the pOptions is updated, up to nOptions.