TCPIP_IPV4_PacketGetSourceAddress Function
C
TCPIP_IPV4_PacketGetSourceAddress(
TCPIP_MAC_PACKET* pPkt
);
Description
The function will return a pointer to where the IPv4 source address is located in the TCPIP_MAC_PACKET. The TCPIP_MAC_PACKET is supposed to be a valid IPv4 packet that has properly source address set.
Preconditions
pPkt - valid IPv4 packet. pNetLayer filed properly set.
Parameters
Parameters | Description |
---|---|
pPkt | Packet to query. |
Returns
- A valid pointer to an IPV$_ADDR - If it succeeds.
- 0 - If call failed.
Remarks
This function is primarily meant for RX packets.