TCPIP_IGMP_ExcludeSource Function
C
TCPIP_IGMP_RESULT TCPIP_IGMP_ExcludeSource(
UDP_SOCKET socket,
TCPIP_NET_HANDLE hNet,
IPV4_ADDR mcastAddress,
IPV4_ADDR sourceAddress
);
Description
This function performs the unsubscription of a UDP socket to multicast traffic from one source.
Preconditions
The IGMP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| socket | the UDP multicast socket. |
| hNet | Interface handle. if hNet == 0, then the default interface will be used. |
| mcastAddress | the multicast address to unsubscribe from. It has to be within the IANA specified multicast address range. |
| sourceAddress | destination source for which the socket wants to unsubscribe from. |
Returns
TCPIP_IGMP_OK if - if operation succeeded, otherwise an error code appears.
Remarks
The function supports ASM functionality. It is a shortcut to TCPIP_IGMP_Subscribe(EXCLUDE, 1 source).