TCPIP_IGMP_Unsubscribe Function
C
TCPIP_IGMP_RESULT TCPIP_IGMP_Unsubscribe(
UDP_SOCKET socket,
TCPIP_NET_HANDLE hNet,
IPV4_ADDR mcastAddress,
const IPV4_ADDR* sourceList,
size_t* listSize
);
Description
This function removes the subscription of a UDP socket to multicast traffic sources. Following this call, the IGMP module will inform network routers of the host updates regarding the multicast traffic.
Preconditions
The IGMP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| socket | The UDP multicast socket. |
| hNet | Interface handle. if hNet == 0, then the default interface will be used. |
| mcastAddress | The multicast group address to unsubscribe from. It has to be within the IANA specified multicast address range. |
| filterMode | Filter type required for this subscription: include/exclude. |
| sourceList | Array of destination sources from which the socket requires unsubscription. |
| listSize | The number of sources in the sourceList array. On input, if listSize == 0 or *listSize == 0, then no sources will be considered and sourceList will be ignored. On output, if listSize != 0, it will contain the number of new sources removed. |
Returns
TCPIP_IGMP_OK - if operation succeeded. An error code otherwise.
Remarks
The function supports both SSM and ASM functionality. The function removes the subscription to the sources no matter the filter mode. If sourceList is empty, then unsubscribe all sources for this (G, socket) pair will be performed. This call is equivalent to Subscribe(INCLUDE, {}).