TCPIP_IGMP_GroupSet Function
C
TCPIP_IGMP_RESULT TCPIP_IGMP_GroupsGet(
IPV4_ADDR* groupsList,
int listSize,
int* pnGroups
);
Description
This function returns the current list of the multicast groups that are subscribed with IGMP. Additional details about a specific group could be optained with TCPIP_IGMP_GroupInfoGet.
Preconditions
The IGMP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| groupsList | Pointer to an array of IPv4 addresses that will receive the subscribed multicast groups. Could be NULL if listSize == 0. |
| listSize | The number of entries in the groupsList array. If 0, the groupsList will not be used/populated. |
| pnGroups | Address to store the number of all subscribed groups. Could be NULL if not needed. |
Returns
TCPIP_IGMP_OK if - if the call succeeds and the pInfo is populated.
TCPIP_IGMP_GROUP_INVALID - if no such multicast group exists.
TCPIP_IGMP_ARG_ERROR - pInfo is NULL.
TCPIP_IGMP_IF_ERROR - no such interface.
Remarks
None.