TCPIP_IGMP_IncludeSource Function
C
TCPIP_IGMP_RESULT TCPIP_IGMP_IncludeSource(
UDP_SOCKET socket,
TCPIP_NET_HANDLE hNet,
IPV4_ADDR mcastAddress,
IPV4_ADDR sourceAddress
);
Description
This function performs the subscription of a UDP socket to multicast traffic for one source.
Preconditions
The IGMP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| socket | The UDP multicast socket. |
| hNet | Interface handle. if hNet == 0, then the default interface will be used. |
| mcastAddress | The multicast address to subscribe to. It has to be within the IANA specified multicast address range. |
| sourceAddress | Destination for source for which the socket wants to listen. |
Returns
TCPIP_IGMP_OK - if operation succeeded. An error code otherwise.
Remarks
The function supports both SSM and ASM functionality. It is a shortcut to TCPIP_IGMP_Subscribe(INCLUDE, 1 source).