TCPIP_IGMP_GroupInfoGet Function
C
TCPIP_IGMP_RESULT TCPIP_IGMP_GroupInfoGet(
TCPIP_NET_HANDLE hNet,
IPV4_ADDR mcastAddress,
TCPIP_IGMP_GROUP_INFO* pInfo
);
Description
This function returns current info about a multicast group status on a specified interface.
Preconditions
The IGMP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| hNet | interface handle for which the query is made. if 0, the default interface will be used. |
| mcastAddress | the multicast group for which the query is made. |
| pInfo | Pointer to a TCPIP_IGMP_GROUP_INFO structure that contains in/out parameters. See the description of TCPIP_IGMP_GROUP_INFO. |
Returns
TCPIP_IGMP_OK if - if the call succeeds and the pInfo is populated.
TCPIP_IGMP_GROUP_INVALID - if no such multicast group exists.
TCPIP_IGMP_ARG_ERROR - pInfo is NULL.
TCPIP_IGMP_IF_ERROR - no such interface.
Remarks
None.