TCPIP_IGMP_Leave Function
C
TCPIP_IGMP_RESULT TCPIP_IGMP_Leave(
UDP_SOCKET socket,
TCPIP_NET_HANDLE hNet,
IPV4_ADDR mcastAddress
);
Description
This function performs the IGMPv2 style "leave" operation for a UDP socket from a multicast group.
Preconditions
The IGMP module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| socket | The UDP multicast socket. |
| hNet | Interface handle. if hNet == 0, then the default interface will be used. |
| mcastAddress | The multicast address to join to. It has to be within the IANA specified multicast address range. |
Returns
TCPIP_IGMP_OK - if operation succeeded. An error code otherwise.
Remarks
The function is an ASM helper. It is a shortcut to TCPIP_IGMP_Subscribe(EXCLUDE, {}).