TCPIP_SMTPC_MODULE_CONFIG Structure
C
typedef struct {
int nMailConnections;
uint32_t serverReplyTmo;
uint32_t serverDataTmo;
uint32_t tlsHandshakeTmo;
int nMailRetries;
uint32_t serverRetryTmo;
uint32_t smtpcRetryTmo;
uint16_t sktTxBuffSize;
uint16_t sktRxBuffSize;
} TCPIP_SMTPC_MODULE_CONFIG;
Description
Structure: TCPIP_SMTPC_MODULE_CONFIG.
This data structure describes the SMTPC configuration data. It is presented to the module as part of the module initialization.
Parameters
| Parameters | Description |
|---|---|
| nMailConnections | Number of mail connections to be created each mail message to be sent requires a mail connection adjust based on the number of simultaneous mail messages in transit. |
| serverReplyTmo | General server response timeout, in seconds. Should be adjusted according to the server responsivity RFC specifies it as 5 min. |
| serverDataTmo | Server response timeout to acknowledge a received mail body/data, in seconds. Should be adjusted according to the server responsivity RFC specifies it as 10 min. |
| tlsHandshakeTmo | Secure connection establishment timeout, in seconds, usually few seconds. |
| nMailRetries | How many times to retry sending a failed mail message. Retries occur only for server reported transient errors. Could be 0 if only one mail send is to be attempted, without retries. |
| serverRetryTmo | The retry interval because of a server transient error, in seconds. RFC specifies it should be at least 30 min. |
| smtpcRetryTmo | The retry interval because of a SMTPC temporary error, in seconds. These include temporary errors related to: DNS, socket connection, TLS. |
| sktTxBuffSize | Size of TX buffer for the associated socket; leave 0 for default. |
| sktRxBuffSize | Size of RX buffer for the associated socket; leave 0 for default. |
Remarks
None.