TCPIP_SMTPC_MailMessage Function
C
TCPIP_SMTPC_MESSAGE_HANDLE TCPIP_SMTPC_MailMessage(
const TCPIP_SMTPC_MAIL_MESSAGE* pMailMessage,
TCPIP_SMTPC_MESSAGE_RESULT* pRes
);
Description
This function sends a mail message to the specified server.
Preconditions
SMTPC module should have been initialized.
Parameters
| Parameters | Description |
|---|---|
| pMailMessage | Pointer to a TCPIP_SMTPC_MAIL_MESSAGE describing the mail message to be sent. |
| pRes | Address to store the operation result. If the call failed, additional info will be reported with this result. Can be NULL if not needed. |
Returns
A valid handle (!= 0) - If mail message scheduled successfully.
0 - If call failed.
Error code otherwise.
Remarks
The returned handle is valid until the final mail notification function is called (TCPIP_SMTPC_MESSAGE_CALLBACK()), if exists, or until the mail transaction is completed. After that the messageHandle is no longer valid and should not be used again.