TCPIP_DHCPS_IsEnabled Function
C
bool TCPIP_DHCPS_IsEnabled(TCPIP_NET_HANDLE hNet)
Description
Determines if the DHCP Server is enabled on the specified interface.
This function returns the current state of the DHCP Server on the specified interface.
Precondition
The DHCP Server module must be initialized.
Parameters
Parameters | Description |
---|---|
hNet | Interface to query |
Returns
- true - server is enabled on the selected interface
- false - server is disabled; or wrong interface, service is down, etc.
Remarks
In multi-threaded environments the returned information is info only and can change at any time.