TCPIP_DHCPS_HandlerDeRegister Function
C
bool TCPIP_DHCPS_HandlerDeRegister(TCPIP_DHCPS_EVENT_HANDLE hDhcp)
Description
Deregisters a previously registered DHCP handler.This function deregisters the DHCP event handler.
Precondition
The DHCP module must be initialized.
Parameters
Parameters | Description |
---|---|
hDhcp | A handle returned by a previous call to TCPIP_DHCPS_HandlerRegister. |
Returns
- true - if the call succeeds
- false - if no such handler is registered