TCPIP_DHCPS_INTERFACE_CONFIG Structure
C
typedef struct
{
uint8_t ifIndex;
uint8_t configFlags;
uint16_t leaseEntries;
uint32_t leaseDuration;
uint32_t minLeaseDuration;
uint32_t maxLeaseDuration;
uint32_t unreqOfferTmo;
const char* serverIPAddress;
const char* startIPAddress;
size_t prefixLen;
const TCPIP_DHCPS_CLIENT_OPTION_CONFIG* pOptConfig;
uint16_t nOptConfigs;
}TCPIP_DHCPS_INTERFACE_CONFIG;
Description
Structure: TCPIP_DHCPS_INTERFACE_CONFIG
DHCP server configuration for a specific interface.
DHCP server configuration and network initialization data. Configuration is part of tcpip_stack_init.c.
Members
Members | Description |
---|---|
ifIndex | interface number to which this configuration refers to |
configFlags | a TCPIP_DHCPS_CONFIG_FLAGS value |
leaseEntries | max number of leases for this interface |
Must be <= TCPIP_DHCPS_MAX_LEASES | |
leaseDuration | default lease duration to be granted to clients, seconds |
minLeaseDuration | minimum lease duration that can be requested by a client, seconds |
if 0, then a default of 60 seconds will be used | |
should be <= leaseDuration | |
maxLeaseDuration | maximum lease duration that can be requested by a client, seconds |
if 0, then the leaseDuration will be used | |
should be >= leaseDuration | |
unreqOfferTmo | timeout for unrequested offer sent to the client, seconds |
Note: used if TCPIP_DHCPS_CONFIG_FLAG_KEEP_UNREQ_OFFERS is not set | |
if 0, a default of 5 seconds will be used | |
serverIPAddress | server IP address on this interface |
startIPAddress | start lease IP address |
the pool of addresses will be | |
where endIPAddress is given by the prefixLen | |
prefixLen | the number of the leading 1 bits in the network mask |
number <= 32 | |
the address is specified in the CIDR format: add/prefix_len | |
the maximum size of the pool is dictated by the prefixLen | |
For example: 192.168.0.0/24 will have 254 leases available | |
(192.168.0.0 and 192.168.0.255 are excluded) | |
and endIPAddress == 192.168.0.254 | |
Note: the number of possible leases == min(leaseEntries, endIPAddress - startIPAddress). | |
The number of leases derived from startIPAddress/prefixLen should be > leaseEntries. | |
pOptConfig | pointer to array of client options for the DHCP server |
nOptConfigs | number of option configurations in the pOptConfig array |