MAC_DRVR_StatisticsGet Function
C
TCPIP_MAC_RES MAC_DRVR_StatisticsGet(
DRV_HANDLE hMac,
TCPIP_MAC_RX_STATISTICS * pRxStatistics,
TCPIP_MAC_TX_STATISTICS * pTxStatistics
);
Returns
TCPIP_MAC_RES_OK if all processing went on OK.
TCPIP_MAC_RES_OP_ERR error code if function not supported by the driver.
Description
This function will get the current value of the statistic counters maintained by the MAC driver.
Remarks
The reported values are info only and change dynamically.
Preconditions
MAC_DRVR_Initialize() should have been called.
MAC_DRVR_Open() should have been called to obtain a valid handle.
Parameters
Parameters | Description |
---|---|
hMac | handle identifying the MAC driver client |
pRxStatistics | Pointer to a TCPIP_MAC_RX_STATISTICS that will receive the current RX statistics counters Can be NULL if not needed |
pTxStatistics | Pointer to a TCPIP_MAC_TX_STATISTICS that will receive the current TX statistics counters Can be NULL if not needed |