MAC_DRVR_Status Function

C

SYS_STATUS MAC_DRVR_Status( SYS_MODULE_OBJ object );

Returns

  • SYS_STATUS_READY - Indicates that any previous module operation for the specified module has completed

  • SYS_STATUS_BUSY - Indicates that a previous module operation for the specified module has not yet completed

  • SYS_STATUS_ERROR - Indicates that the specified module is in an error state

Description

This function provides the current status of the MAC driver module.

Remarks

None

Preconditions

The MAC_DRVR_Initialize() function must have been called before calling this function.

Parameters

ParametersDescription
objectDriver object handle, returned from MAC_DRVR_Initialize