TCPIP_DHCPV6_SERVER_STATUS_CODE Enumeration

C

typedef enum {
TCPIP_DHCPV6_SERVER_STAT_SUCCESS = 0,
TCPIP_DHCPV6_SERVER_STAT_UNSPEC_FAIL = 1,
TCPIP_DHCPV6_SERVER_STAT_NO_ADDRS_AVAIL = 2,
TCPIP_DHCPV6_SERVER_STAT_NO_BINDING = 3,
TCPIP_DHCPV6_SERVER_STAT_NOT_ON_LINK = 4,
TCPIP_DHCPV6_SERVER_STAT_USE_MULTICAST = 5,
TCPIP_DHCPV6_SERVER_STAT_MAX_CODE = 5,
TCPIP_DHCPV6_SERVER_STAT_EXT_ERROR = -1
} TCPIP_DHCPV6_SERVER_STATUS_CODE;

Description

DHCPv6 server status code.

Members

MembersDescription
TCPIP_DHCPV6_SERVER_STAT_SUCCESS = 0Success.
TCPIP_DHCPV6_SERVER_STAT_UNSPEC_FAIL = 1Failure, reason unspecified; this status code is sent by either a client or a server to indicate a failure not explicitly specified in the RFC.
TCPIP_DHCPV6_SERVER_STAT_NO_ADDRS_AVAIL = 2Server has no addresses available to assign to the IA(s).
TCPIP_DHCPV6_SERVER_STAT_NO_BINDING = 3Client record (binding) unavailable.
TCPIP_DHCPV6_SERVER_STAT_NOT_ON_LINK = 4The prefix for the address is not appropriate for the link to which the client is attached.
TCPIP_DHCPV6_SERVER_STAT_USE_MULTICAST = 5Sent by a server to a client to force the client to send messages to the server using the All_DHCP_Relay_Agents_and_Servers address.
TCPIP_DHCPV6_SERVER_STAT_MAX_CODE = 5Maximum valid value.
TCPIP_DHCPV6_SERVER_STAT_EXT_ERROR = -1An error occurred, status code not found, etc.