The following are the two parameters to consider for the CSEQ write Flash Request:
Offset of the firmware data to
send
Firmware data
The maximum limit for the firmware data is 240 bytes. After Flashing the firmware by the BM78 or the RN4678 module, the BM78 or the RN4678 module returns an CSEQ Event. The CSEQ Event
consists of the firmware offset and the firmware data length.
The following figure illustrates the Write Flash Request Event example data and the CSEQ
Response. In the CSEQ event, the 0x0000 is the previous firmware data offset and 0x20 is
the data length of the firmware chunk; see the following figure.Figure 5-13. Write Flash Request Event
Example Data