6.5 LED Driver
The IS20xxS SoC consists of two LED drivers to control the LEDs. The LED drivers provide enough sink current (16-step control and 0.35 mA for each step) and the LED is connected directly to the IS20xxS SoC.
Note: Configure the LED settings using the IS20XXS_UI tool.
The following figure illustrates the LED driver in the IS20xxS SoC.