10.1.7.11 12-bit ADC Characteristics

Table 10-54. ADC Power Supply and Voltage Reference Input Characteristics
SymbolParameterConditionsMinTypMaxUnit
VDDANASupply voltage range (VDDANA)–3.0–3.6V
IVDDANACurrent consumption on VDDANA(2)Low Speed – fS ≤ 500 kS/s

ADC_ACR.IBCTL = (00)2

–0.71.0mA
Full Speed – fS ≤ 1 MS/s

ADC_ACR.IBCTL = (01)2

–1.21.7mA
VADVREFPADVREFP input voltage range(1)–2.4–VDDANAV
RADVREFPADVREFP input resistance to ground(2)ADC on7.2–12kΩ
ADC off1––MΩ
CADVREFPRecommended decoupling capacitor on ADVREFP–1––μF
Note:
  1. ADVREFN pin must be connected to the PCB ground plane.
  2. Simulation data

Table 10-55. ADC Timing Characteristics
SymbolParameterConditionsMinTypMaxUnit
fCKADCADC clock frequencyADC_ACR.IBCTL = (00)20.1–10MHz
ADC_ACR.IBCTL = (01)20.2–20MHz
tCONVADC conversion time(1)–20––tCKADC
fSSampling rate(2)ADC_ACR.IBCTL = (00)2––0.5MS/s
ADC_ACR.IBCTL = (01)2––1MS/s
tSTARTStartup time(4)Off to on––5μs
tTRACKTrack and hold time(3)–300––ns
Note:
  1. tCONV = tCH + tTRACK + 14 x tCKADC with tCKADC = 1 / fCKADC. tCH = 0 when the ADC operates in the same input mode (single-ended, pseudo-differential or differential) for the current conversion than for the previous one. tCH = 2 when the ADC input mode is changed to perform the current conversion.
  2. fS = 1 / tCONV.
  3. See Track and Hold Time versus Source Impedance – Sampling Rate.
  4. Simulation data

Table 10-56. ADC Analog Input Characteristics
SymbolParameterConditionsMinTypMaxUnit
VFSAnalog input full scale range(1)ADC_CCR.DIFFx = 00–VADVREFV
ADC_CCR.DIFFx = 1-VADVREF–VADVREFV
VINCMCommon mode input range in Differential Input mode(2)ADC_CCR.DIFFx = 10.4 x VDDANA–0.6 x VDDANAV
CSADC sampling capacitance(5) –––3pF
CP_ADxADx input parasitic capacitance(3)(5)ADx pin configured as analog input––7pF
RONInternal series resistor(3)(5)–––2kΩ
ZINCommon mode input impedance(4)(5)On ADx pin1 / (fS.CS)––Ω
Note:
  1. VFS = (VADx - VGNDANA) in Single-ended mode, VFS = (VADx - VAD11) in Pseudo-differential mode, and VFS = (VADx - VADx+1) in Differential mode.
  2. VINCM = (VADx + VADx+1) / 2.
  3. With respect to the equivalent model of figure Equivalent Model of the Acquisition Path.
  4. Assuming conversion on one single channel
  5. Simulation data

Figure 10-41. Acquisition Path Block Diagram

For tracking time calculation, during the sampling phase of the converter, this acquisition path can be reduced to the equivalent model provided in the following figure, where:

  • RON = RMUX + RS
  • CP_ADX = CPX + CP_MUX

Figure 10-42. Equivalent Model of the Acquisition Path

See Track and Hold Time versus Source Impedance – Sampling Rate for further details on how to use this model.

In the following table, unless otherwise specified, the specifications are given for two speed operating ranges.
  • Source resistance = 50 Ω
  • ADC_EMR.OSR<2:0> = (000)2
  • Low-speed
    • fCKADC = 10 MHz, fS = 500 kS/s
    • ADC_ACR.IBCTL = (00)2
  • High-speed
    • fCKADC = 20 MHz, fS = 1 MS/s
    • ADC_ACR.IBCTL = (01)2

Table 10-57. Static Performance Characteristics(1)
SymbolParameterConditionsMinTypMaxUnit
RESADCNative ADC resolution––12–Bit
INLIntegral non-linearitySingle mode-3–+3LSB
Differential mode(3)-2–+2LSB
DNLDifferential non-linearitySingle mode-2–+2LSB
Differential mode(3)-1+1LSB
OEOffset error(2)–-4–4LSB
GEGain error(2)–-4–4LSB
Warning: ADC channels should be selected knowing that toggling the QSPI I/Os may decrease ADC channel 4 and 0 performances.
Note:
  1. In this table, errors are expressed in LSB where:
    • LSB = VADVREF / 212 in Single-ended mode (ADC_CCR.DIFFx = 0 and ADC_PDR.PDIFFx = 0)
    • LSB = VADVREF / 211 in Differential or Pseudo-differential mode (ADC_CCR.DIFFx = 1)
  2. Error with respect to the best fit line method.
  3. Simulation data