2.1 Immobilizer Block
The immobilizer is considered the system foundation because it must always work, even if the fob battery is dead, and secures a vehicle against unauthorized engine starts. It consists of a base station, placed in the vehicle, that provides the LF (125 kHz) magnetic field enabling a wireless link with the transponder in the fob to be established. This LF immobilizer link is used to exchange the power supply and digital data between the vehicle and the passive transponder.
The implemented immobilizer system supports Microchip’s OIP, which consists of an open/unlicensed
protocol stack based on AES-128 encryption. First, the ReadUID command is
sent to the fob. The fob has to decode the ReadUID command and respond with
its Unique ID (UID) value. If the received UID value is correct (matches the stored UID), the
start authentication command is issued and challenge data is sent to the fob based on the
authentication type (unilateral or bilateral). The fob receives the challenge, performs the
encryption and sends a ciphered response back. This response is received by the base station
and verified to complete the authentication process.
- The fob is a receive-only device; therefore, the ciphered response back to the base station is accomplished by loading/unloading the magnetic field to encode the data.
- For more details on the OIP protocol, refer to the ATAN0088 Open Source Immobilizer Protocol Stack Application Note (9195).