5.14.3.3 The #pragma Inline Directive
The #pragma inline directive indicates to the compiler
that calls to the specified function should be as fast as possible. This pragma has the
same effect as using the inline function specifier.