5.2.4 Configuration Bit Access
The pragma allows the configuration bits (or
fuses) and ID-location registers to be specified in the assembly source file.
Configuration bits, or fuses, are used to set up fundamental device operation, such as
the oscillator mode, watchdog timer, programming mode and code protection. These bits
must be correctly set to ensure your program executes correctly.config
The pragma has the following forms:
#pragma config setting = value
#pragma config register = literal_value
setting is a configuration setting descriptor,
e.g., WDT, and value can be either a
textual description of the desired state, e.g., OFF, or a numerical
value. Either the setting or
value tokens or the
setting = value expression
can be surrounded by either double or single quotes to protect them from any macro
substitution performed by the preprocessor, for
example:#pragma config "WDT = ON" // turn on watchdog timer
#pragma config WDTPS = 0x1A // specify the timer postscale valuevalue tokens that appear to be purely numerical are in fact a
textual description of the value, for example in the
following:config WDTPS = 32the 32 token is a
textual description for some devices that indicates a watchdog timer post-scale of 1:32,
not the number 32. In such a case, it might not be the number 32 that is programmed into
the relevant bits of the configuration register. The assembler will first check if
value represents a predefined string, and only
if that is not the case, assume it represents a numerical constant, which will then be
subject to the same constraints as other numerical constant operands.You should never assume that the OFF and
ON tokens used in configuration macros equate to 0 and 1,
respectively, as that is often not the case.
The register field is the name of a configuration or
ID-location register, and this must always be used with a
value that is a numerical constant, for
example:
#pragma config CONFIG1L = 0x8F
The available setting,
register and
value fields are documented in the chipinfo file
relevant to your device (i.e. pic_chipinfo.html and
pic18_chipinfo.html) and that are located in the
docs directory of your compiler installation. Click the link to
your target device and the page will show you the settings and values that are
appropriate with this pragma. Configuration registers that are One-Time-Programmable are
indicated next to the register's name in these files. Review your device data sheet for
more information.
One config pragma can be used to set each configuration setting;
alternatively, several comma-separated configuration settings can be specified by the
same pragma. The pragma can be used as many times as required to fully configure the
device.
// PIC18F67K22
// VREG Sleep Enable bit : Enabled
// LF-INTOSC Low-power Enable bit : LF-INTOSC in High-power mode during Sleep
// SOSC Power Selection and mode Configuration bits : High Power SOSC circuit selected
// Extended Instruction Set : Enabled
#pragma config RETEN = ON, INTOSCSEL = HIGH, SOSCSEL = HIGH, XINST = ON
// Alternatively
#pragma config CONFIG1L = 0x5D
// IDLOC @ 0x200000
#pragma config IDLOC0 = 0x15The config pragmas do not produce executable code and
ideally, they should be placed outside function definitions. Avoid placing these pragmas
in library archives, as they do not define symbols and hence will not normally be linked
into the application. It is recommended that these pragmas be placed in one C source
file. Be mindful when merging bootloader and application projects that these pragmas
should be defined by only one of these projects.
All the bits in the Configuration Words should be programmed to prevent erratic program behavior. Do not leave them in their default/unprogrammed state. Not all Configuration bits have a default state of logic high; some have a logic low default state. Consult your device data sheet for more information.
If you are using MPLAB X IDE, take advantage of its built-in tools to generate the required pragmas, so that you can copy and paste them into your source code. See the MPLAB® X IDE User’s Guide for a description and use of the Configuration Bits window.