5.2.6 Program Memory Symbols
Microchip PIC18 devices typically have various regions in their program memory address
space in addition to the program flash memory (PFM). These regions contain device and
configuration information of utility to user projects, and can be read using table
reads, the same mechanism employed by the compiler to read constant data stored in PFM.
The compiler defines special extern const symbols mapped to these
regions in the device-specific headers. These symbols can be used by C programs to
easily read the contents of these regions and are available once you include
<xc.h> in your source files. The regions represented and
examples symbols defined for these regions are described below.
#pragma config directive (see Configuration Bit Access). The following are
examples of the compiler-provided symbol definitions representing user ID
locations.extern const unsigned _IDLOCs[8] __at(0x200000);
extern const unsigned _IDLOC0 __at(0x200000);
extern const unsigned _IDLOC1 __at(0x200002);
extern const unsigned _IDLOC2 __at(0x200004);So, for example, the
_IDLOC1 C variable could be used to read the second User ID
location.#pragma config directive. The following are examples of the
compiler-provided symbol definitions representing Configuration Word
locations.extern const unsigned char _CONFIGs[10] __at(0x300000);
extern const unsigned char _CONFIG1L __at(0x300000);
typedef union {
struct {
unsigned FEXTOSC :3;
unsigned :1;
unsigned RSTOSC :3;
};
} _CONFIG1Lbits_t;
extern const _CONFIG1Lbits_t _CONFIG1Lbits __at(0x30000);
extern const unsigned char _CONFIG1H __at(0x300001);
typedef union {
struct {
unsigned CLKOUTEN :1;
unsigned PR1WAY :1; unsigned CSWEN :1;
unsigned FCMEN :1;
};
} _CONFIG1Hbits_t;
extern const _CONFIG1Hbits_t _CONFIG1Hbits __at(0x30001);So, for example,
the _CONFIG1Lbits.FEXTOSC bit-field could be used to read the External
Oscillator Selection configuration bits.extern const unsigned _DIA[32] __at(0x3F0000);
extern const unsigned _DIA_MUI[8] __at(0x3F0000);
extern const unsigned _DIA_MUI0 __at(0x3F0000);
extern const unsigned _DIA_MUI1 __at(0x3F0002);
extern const unsigned _DIA_MUI2 __at(0x3F0004);
extern const unsigned _DIA_EUI[10] __at(0x3F0010);
extern const unsigned _DIA_EUI0 __at(0x3F0010);
extern const unsigned _DIA_EUI1 __at(0x3F0012);
extern const unsigned _DIA_EUI2 __at(0x3F0014);So, for example, the
_DIA_MUI1 C variable could be used to read the second Microchip
Unique Identifier.extern const unsigned _DCI[5] __at(0x3FFF00);
extern const unsigned _DCI_ERSIZ __at(0x3FFF00);
extern const unsigned _DCI_WLSIZ __at(0x3FFF02);
extern const unsigned _DCI_URSIZ __at(0x3FFF04);
extern const unsigned _DCI_EESIZ __at(0x3FFF06);
extern const unsigned _DCI_PCNT __at(0x3FFF08);So, for example, the
_DCI_WLSIZ C variable could be used to read the number of write
latches per row information.extern const unsigned _DEVID __at(0x3FFFFE);
extern const unsigned _REVID __at(0x3FFFFC);So, for example, the
_REVID C variable could be used to read the revision ID.