37.3.7.6 Affine to Projective Coordinates Conversion

Purpose

This service is used to perform a point coordinates conversion from an affine point representation to projective.

How to Use the Service

Description

The operation performed is:

affine(Xa, Ya) → projective(Xp, Yp, Zp)

In this computation, the following parameters need to be provided:

  • A the input point is filled in affine coordinates for X and Y, and setting Z to 1 (pointed by {nu1PointABase,3*u2ModLength + 4}).
  • Cns the Fast Modular Constant filled (pointed by {nu1CnsBase,u2ModLength + 8})
  • P the modulus filled (pointed by {nu1ModBase,u2ModLength + 4})
  • The workspace not initialized (pointed by {nu1WorkSpace, 2*u2ModLength +16} The result is the point A with its (X,Y,Z) projective coordinates.

The service name for this operation is GF2NEcConvAffineToProjective.

Important: Before using this service, ensure that the constant Cns has been calculated with the setup of the Fast Modular Reductions service.

Parameters Definition

Table 37-102. GF2NEcConvAffineToProjective Service Parameters
ParameterTypeDirectionLocationData LengthBefore Executing the ServiceAfter Executing the Service
nu1ModBasenu1ICrypto RAMu2ModLength + 4Base of modulus PBase of modulus P
nu1CnsBasenu1ICrypto RAMu2ModLength + 8Base of CnsBase of Cns
u2ModLengthu2I––Length of modulus PLength of modulus P
nu1PointABasenu1ICrypto RAM3*u2ModLength + 12Input point AResulting point A in affine coordinates
nu1Workspacenu1ICrypto RAM2*u2ModLength + 16–Workspace

Code Example

PUKCL_PARAM PUKCLParam;
PPUKCL_PARAM pvPUKCLParam = &PUKCLParam;

// ! The Random Number Generator must be initialized and started
// ! following the directives given for the RNG on the chip

PUKCL (u2Option) = 0;

PUKCL _GF2NEcConvAffineToProjective(nu1ModBase) = <Base of the ram location of P>; 
PUKCL _GF2NEcConvAffineToProjective(u2ModLength) = <Byte length of P>;
PUKCL _GF2NEcConvAffineToProjective(nu1CnsBase) = <Base of the ram location of Cns>;
PUKCL _GF2NEcConvAffineToProjective(nu1PointABase) = <Base of the ram location of the A point>; 
PUKCL _GF2NEcConvAffineToProjective(nu1Workspace) = <Base of the ram location of the workspace>;
...

// vPUKCL_Process() is a macro command, which populates the service name
// and then calls the library...
vPUKCL_Process(GF2NEcConvAffineToProjective,&PUKCLParam); 
if (PUKCL (u2Status) == PUKCL_OK)
            {
            ...
            }
else // Manage the error

Constraints

No overlapping between either input and output are allowed. The following conditions must be avoided to ensure that the service works correctly:

  • nu1ModBase, nu1CnsBase, nu1PointABase, nu1Workspace are not aligned on 32-bit boundaries
  • {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength + 8}, {nu1PointABase, 3*u2ModLength + 12}, {nu1Workspace, <WorkspaceLength>} are not in Crypto RAM
  • u2ModLength is either: < 12, > 0xffc or not a 32-bit length
  • All overlapping between {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength + 8}, {nu1PointABase, 3*u2ModLength + 12}, and {nu1Workspace, 2*u2ModLength + 16}

Status Returned Values

Table 37-103. GF2NEcConvAffineToProjective Service Return Codes
Returned StatusImportanceMeaning
PUKCL_OK–The computation passed without problem.