5.13.1 Monitor LLDP Neighbors
The LLDP Neighbor Information page provides a status overview for all LLDP neighbors. The displayed table contains a row for each interface on which an LLDP neighbor is detected.
The LLDP Neighbor Information page has the following parameters:
- Local Interface: The interface on which the LLDP frame was received
- Chassis ID: The Chassis ID is the identification of the neighbor's LLDP frames
- Port ID: The Port ID is the identification of the neighbor port
- Port Description: Port Description is the port description advertised by the neighbor unit
- System Name: System Name is the name advertised by the neighbor unit
- System Capabilities: System
Capabilities describes the neighbor unit's capabilities. The possible capabilities
are:
- Other
- Repeater
- Bridge
- WLAN Access Point
- Router
- Telephone
- DOCSIS cable device
- Station only
- Reserved
Note: When a capability is enabled, the capability is followed by (+). If the capability is disabled, the capability is followed by (-). - Management Address: Management Address is the neighbor unit's address that is used for higher layer entities to assist discovery by the network management. This can, for example, hold the neighbor's IP address.