5.13.5 Monitor LLDP Port Statistics
The Monitor > LLDP > Port Statistics page provides an overview of all LLDP traffic. Two types of counters are shown. Global counters are counters that refer to the whole switch, while local counters refer to per interface counters for the currently selected switch.
The list of parameters is as follows:
- Global Counters
- Clear global counters: If checked the global counters are cleared when clear is clicked
- Neighbor entries were last changed: Shows the time when the last entry was last deleted or added. It also shows the time elapsed since the last change was detected.
- Total Neighbors Entries Added: Shows the number of new entries added since switch reboot
- Total Neighbors Entries Deleted: Shows the number of new entries deleted since switch reboot
- Total Neighbors Entries Dropped: Shows the number of LLDP frames dropped due to the entry table being full
- Total Neighbors Entries Aged Out: Shows the number of entries deleted due to TLL expiring
- Local Counters
- Local Interface: The interface on which LLDP frames are received or transmitted
- Tx Frames: The number of LLDP frames transmitted on the interface
- Rx Frames: The number of LLDP frames received on the interface
- Rx Errors: The number of received LLDP frames containing an error
- Frames Discarded: If an LLDP frame is received on an interface, and the switch's internal table has run full, the LLDP frame is counted and discarded. This situation is known as Too Many Neighbors in the LLDP standard. LLDP frames require a new entry in the table when the Chassis ID or Remote Port ID is not already contained within the table. Entries are removed from the table when a given interface's link is down, an LLDP shutdown frame is received, or when the entry ages out.
- TLVs Discarded: Each LLDP frame can contain multiple pieces of information, known as Type Length Value (TLVs). If a TLV is malformed, then it is counted and discarded.
- TLVs Unrecognized: The number of well-formed TLVs, but with an unknown type of value.
- Org. Discarded: If LLDP frame is received with an organizationally TLV, but the TLV is not supported the TLV is discarded and counted.
- Age-Outs: Each LLDP frame contains information about how long time the LLDP information is valid (Age-Out time). If no new LLDP frame is received within the age out time, then the LLDP information is removed, and the Age-Out counter is incremented.
- Clear: If checked, the counters for the specific interface are cleared when clear is clicked