5.12.2 Monitor Spanning Tree Port Status
The STP Port Status page displays the STP CIST port status for physical ports of the switch.
The STP Port Status page has the following parameters:
- Port: The switch port number of the logical STP port
- CIST Role: The current STP port role of the CIST port. The port role can be one of the following values: AlternatePort, BackupPort, RootPort, DesignatedPort, and Disabled.
- CIST State: The current STP port state of the CIST port. The port state can be one of the following values: Discarding, Learning, and Forwarding.
- Uptime: The time since the bridge port was last initialized