7.6.6.1 Options For Specific Optimization Control
The following options control specific optimizations. The
-O2 option turns on all of these optimizations except
-funroll-loops, -funroll-all-loops and
-fstrict-aliasing.
You can use the following flags in the rare cases when “fine-tuning” of optimizations to be performed is desired.
| Option | Definition |
|---|---|
-falign-functions
| Align the start of functions to the
next power-of-two greater than n, skipping up to n
bytes. For instance, -falign-functions=32 aligns
functions to the next 32-byte boundary, but
-falign-functions=24 would align to the next
32-byte boundary only if this can be done by skipping 23 bytes or
less.
The
assembler only supports this flag when |
-falign-labels
| Align all branch targets to a
power-of-two boundary, skipping up to n bytes like
-falign-functions. This option can easily make code
slower, because it must insert dummy operations for when the branch
target is reached in the usual flow of the code.If
If |
-falign-loops
| Align loops to a power-of-two boundary,
skipping up to n bytes like
-falign-functions. The hope is that the loop will
be executed many times, which will make up for any execution of the
dummy operations.If |
-fcaller-saves | Enable values to be allocated in registers that will be clobbered by function calls, by emitting extra instructions to save and restore the registers around such calls. Such allocation is done only when it seems to result in better code than would otherwise be produced. |
-fcse-follow-jumps | In common subexpression elimination,
scan through jump instructions when the target of the jump is not
reached by any other path. For example, when CSE encounters an
if statement with an else clause,
CSE will follow the jump when the condition tested is false. |
-fcse-skip-blocks | This is similar to
-fcse-follow-jumps, but causes CSE to follow jumps
which conditionally skip over blocks. When CSE encounters a simple
if statement with no else clause,
-fcse-skip-blocks causes CSE to follow the jump
around the body of the if. |
-fexpensive-
optimizations | Perform a number of minor optimizations that are relatively expensive. |
-ffunction-sections
| Place each function or data item into
its own section in the output file. The name of the function or the name
of the data item determines the section’s name in the output file. Only use these options when there are significant benefits for doing so. When you specify these options, the assembler and linker may create larger object and executable files and will also be slower. See also The |
-fgcse | Perform a global common subexpression elimination pass. This pass also performs global constant and copy propagation. |
-fgcse-lm | When -fgcse-lm is
enabled, global common subexpression elimination will attempt to move
loads which are only killed by stores into themselves. This allows a
loop containing a load/store sequence to be changed to a load outside
the loop, and a copy/store within the loop. |
-fgcse-sm | When -fgcse-sm is
enabled, a store motion pass is run after global common subexpression
elimination. This pass will attempt to move stores out of loops. When
used in conjunction with -fgcse-lm, loops containing a
load/store sequence can be changed to a load before the loop and a store
after the loop. |
-fno-defer-pop | Always pop the arguments to each function call as soon as that function returns. The compiler normally lets arguments accumulate on the stack for several function calls and pops them all at once. |
-fno-peephole
| Disable machine specific peephole
optimizations. Peephole optimizations occur at various points during the
compilation. -fno-peephole disables peephole
optimization on machine instructions, while
-fno-peephole2 disables high level peephole
optimizations. To disable peephole entirely, use both options. |
-foptimize-
register-move
| Attempt to reassign register numbers in
move instructions and as operands of other simple instructions in order
to maximize the amount of register tying.
|
-frename-registers | Attempt to avoid false dependencies in scheduled code by making use of registers left over after register allocation. This optimization will most benefit processors with lots of registers. It can, however, make debugging impossible, since variables will no longer stay in a “home register”. |
-frerun-cse-after-
loop | Rerun common subexpression elimination after loop optimizations has been performed. |
-frerun-loop-opt | Run the loop optimizer twice. |
-fschedule-insns | Attempt to reorder instructions to eliminate Read-After-Write stalls (see your device Family Reference Manual (FRM) for more details). Typically improves performance with no impact on code size. |
-fschedule-insns2 | Similar to
-fschedule-insns, but requests an additional pass
of instruction scheduling after register allocation has been
done. |
-fstrength-reduce | Perform the optimizations of loop strength reduction and elimination of iteration variables. |
-fstrict-aliasing | Allows the compiler to assume the
strictest aliasing rules applicable to the language being compiled. For
C, this
activates optimizations based on the type of expressions. In
particular, an object of one type is assumed never to reside at the same
address as an object of a different type, unless the types are almost
the same. For example, an unsigned int can alias an
int, but not a void* or a
double. A character type may alias any other
type.Pay special attention to code like this: The practice of reading from a different union
member than the one most recently written to (called “type-punning”)
is common. Even with |
-fthread-jumps | Perform optimizations where a check is made to see if a jump branches to a location where another comparison subsumed by the first is found. If so, the first branch is redirected to either the destination of the second branch or a point immediately following it, depending on whether the condition is known to be true or false. |
-funroll-loops | Perform the optimization of loop
unrolling. This is only done for loops whose number of iterations can be
determined at compile time or run time. -funroll-loops
implies both -fstrength-reduce and
-frerun-cse-after-loop. |
-funroll-all-loops | Perform the optimization of loop
unrolling. This is done for all loops and usually makes programs run
more slowly. -funroll-all-loops implies
-fstrength-reduce, as well as
-frerun-cse-after-loop. |