9.9.2 __prog__ Type Qualifier
The __prog__ qualifier is similar to the
__psv__ qualifier (see __psv__ Type Qualifier), but indicates to the
compiler that the qualified variable or pointer target may straddle PSV pages. As a result,
the compiler will generate code so these qualified objects can be read correctly,
regardless of which page they are allocated to. This code may be longer than that to access
variables or pointer targets which are qualified __psv__. For example:
__prog__ unsigned int __attribute__((space(prog))) myPROGvar =
0x1234;
__prog__ char * myPROGpointer;
The pointer in this example does not use the space
attribute as it is located in data memory, but the qualifier indicates how the pointer
targets are to be accessed. For more information on the space attribute
and how to allocate variables to the Flash memory, see Variable Attributes and Address Spaces for basic information
on the memory layout and how program memory is accessed by the device.