1.1.2.1.1.4.61 BLE_GAP_SetPeriAdvRxEnable
C
uint16_t BLE_GAP_SetPeriAdvRxEnable(uint16_t syncHandle, bool enable);Description
Enables or disables reports for the periodic advertising train identified by input "syncHandle".
Note
This API belongs to extended advertising feature. It will be disallowed if any one API that belongs to legacy advertising feature is issued before. Categories of advertising APIs and events for details of advertising APIs.
BLE_GAP_ScanInit, BLE_GAP_ExtScanInit and BLE_GAP_SyncInit are required for this API.
Events generated
BLE_GAP_EVT_PERI_ADV_REPORT Generated when enabled.
Parameters
| Parameter | Description |
|---|---|
| [in] syncHandle | Identity of the periodic advertising train. |
| [in] enable | Enable or disable reports. Set true to enable reports. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully enables or disables reports for the periodic advertising train. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed. |
| MBA_RES_UNKNOWN_ADV_ID | Unknown advertising identifier. |