1.1.2.1.1.4.12 BLE_GAP_EnableOneTimeAdv
C
uint16_t BLE_GAP_EnableOneTimeAdv(uint8_t option);Description
Start one time advertising event.
Note
This API belongs to legacy advertising feature. It will be disallowed if any one API belongs extended advertising feature is issued before. Categories of advertising APIs and events for details of advertising APIs.
BLE_GAP_AdvInit is required for this API.
Events generated
BLE_GAP_EVT_CONNECTED Generated when connection is established. BLE_GAP_EVT_ADV_COMPL Generated when advertising event is complete.
Only one of aboved events would be generated at the same time.
Parameters
| Parameter | Description |
|---|---|
| [in] option | Option for one time advertising. See Advertising option. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully start advertising. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | Invalid parameters. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed when extended Adv. feature is in-use. |