1.1.2.1.1.4.60 BLE_GAP_SetPeriAdvParams
C
uint16_t BLE_GAP_SetPeriAdvParams(BLE_GAP_PeriAdvParams_T *p_periAdvParams);Description
Configure periodic advertising parameters.
Note
If the advHandle does not identify an advertising set that is already configured for periodic advertising and it is unable to support more periodic advertising at present.
This API belongs to extended advertising feature. It will be disallowed if any one API that belongs to legacy advertising feature is issued before. Categories of advertising APIs and events for details of advertising APIs.
BLE_GAP_AdvInit, BLE_GAP_ExtAdvInit and BLE_GAP_PeriodicAdvInit are required for this API.
Parameters
| Parameter | Description |
|---|---|
| [in] p_periAdvParams | Pointer to BLE_GAP_PeriAdvParams_T structure buffer. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully configure periodic advertising parameters. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | Invalid parameters. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed. |
| MBA_RES_UNKNOWN_ADV_ID | Unknown advertising identifier. |