1.1.2.1.1.4.62 BLE_GAP_SetPhy
C
uint16_t BLE_GAP_SetPhy(uint16_t connHandle, uint8_t txPhys, uint8_t rxPhys, uint8_t phyOptions);Description
Set the PHY preferences for the specified connection.
Note
The Controller might not be able to make the change. Event will generate if one of the phy changes.
Events generated
BLE_GAP_EVT_PHY_UPDATE Generated when phy updated.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | Connection handle associated with this connection. |
| [in] txPhys | TX PHYs. A bit field that indicates the transmitter PHYs that the user prefers to use. See PHY option for transmit and receive. |
| [in] rxPhys | RX PHYs. A bit field that indicates the receiver PHYs that the user prefers to use. See PHY option for transmit and receive. |
| [in] phyOptions | PHY options. See Preferred PHY preference. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully set the PHY preferences for the specified connection. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | Invalid parameters. |
| MBA_RES_UNKNOWN_CONN_ID | Unknown connection identifier. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed. |