1.1.2.1.1.4.59 BLE_GAP_SetPeriAdvEnable
C
uint16_t BLE_GAP_SetPeriAdvEnable(bool enable, uint8_t advHandle);Description
Enable or disable the periodic advertising for the advertising set specified by the advHandle.
Note
If the advertising set is not currently enabled (see BLE_GAP_SetExtAdvEnable API), the periodic advertising is not started until the advertising set is enabled.
The periodic advertising should continue until this API is called with enable set to false.
This API belongs to extended advertising feature. It will be disallowed if any one API that belongs to legacy advertising feature is issued before. Categories of advertising APIs and events for details of advertising APIs.
BLE_GAP_AdvInit, BLE_GAP_ExtAdvInit and BLE_GAP_PeriodicAdvInit are required for this API.
Parameters
| Parameter | Description |
|---|---|
| [in] enable | Enable or disable the periodic advertising. |
| [in] advHandle | Identifies which advertising set to be enabled or disabled. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully enable or disable the periodic advertising. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | Invalid parameters. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed. |
| MBA_RES_UNKNOWN_ADV_ID | Unknown advertising identifier. |