1.1.2.1.1.4.66 BLE_GAP_SetScanningParam
C
uint16_t BLE_GAP_SetScanningParam(BLE_GAP_ScanningParams_T *p_scanParams);Description
Set the Scanning Parameters.
Note
This API should not be called when scanning is enabled.
This API belongs to legacy advertising feature. It will be disallowed if any one API belongs extended advertising feature is issued before. Categories of advertising APIs and events for details of advertising APIs.
BLE_GAP_ScanInit is required for this API.
Parameters
| Parameter | Description |
|---|---|
| [in] p_scanParams | Pointer to BLE_GAP_ScanningParams_T structure buffer. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully set scanning parameters. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | Invalid parameters, if any of the scanning parameters are out of range. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed when extended Adv. feature is in-use. |