OTA_SERVICE_FH_StateGet
C
OTA_SERVICE_FH_STATE OTA_SERVICE_FH_StateGet(void)
Summary
Returns the current state of the File handler state machine.
Description
This function can be used to poll the current state of the File handler state machine
Precondition
None.
Parameters
None.
Returns
Returns the current state of the File handler. One of the value of OTA_SERVICE_FH_STATE enum
Example
if (OTA_SERVICE_FH_StateGet() == OTA_SERVICE_FH_STATE_IDLE)
{
// Idle state
}
Remarks
None.