2.9 Data Byte Count
The data byte count is the number of bytes in a complete I2C packet. The I2CxCNT register is used to specify the length, in bytes, of the complete transaction. The value loaded into I2CxCNT will decrement each time a data byte is transmitted or received by the module.
When a byte transfer causes the I2CxCNT register to decrement to
‘0’, the Byte Count Interrupt Flag (CNTIF) bit of the I2CxPIR
register is set, and if the Byte Count Interrupt Enable (CNTIE) bit is also set, the
general purpose I2C Interrupt Flag (I2CxIF) bit is set. The I2CxIF is a read-only bit
and can only be cleared by clearing all Enabled Interrupt Flag bits in the I2CxPIR
register.
The I2CxCNT register can be read at any time, but it is recommended that a double read is performed to ensure a valid read.
The I2CxCNT register can be written to, but care is required to prevent register
corruption. If the I2CxCNT register is written to during the 8th falling SCL edge during
reception, or during the 9th falling SCL edge during transmission, the register value
may be corrupted. In Client mode, I2CxCNT can be safely written to any time the client
is stretching the clock (CSTR = 1), or after a Stop condition has been
received. If the I2C packet is longer than 255 bytes, the I2CxCNT value can
be updated mid-message to prevent the count from reaching ‘0’; however,
the preventative measures listed above must be followed.
The I2CxCNT value can be automatically loaded when the Auto-Load I2C Count Register Enable (ACNT) bit of the I2CxCON2 register is set. When ACNT is set, the data byte following the address byte is loaded into I2CxCNT, and the value of the Acknowledge Data (ACKDT) bit is used for the ACK response.
When in either Client-Read or Host-Write mode and the I2CxCNT value is not
‘0’, the value of the ACKDT bit is used for the
ACK response. When I2CCNT = 0, the value
of the Acknowledge End of Count (ACKCNT) bit is used for the
ACK response.