6.2.3.1 rlmadduser – add a user to the ISV server options file
Usage: rlmadduser options-filename username password
This command adds the specified username/password pair to the end of the options-file specified.
Note:
- Usernames and passwords must be <= 10 characters long
- Usernames and passwords are CASE SENSITIVE
- Usernames and passwords cannot contain white space or any of the following
characters:
"<", ">", "&", “:”, and single (''' or '`') or double-quotes (")
- If there are no USER records in the ISV server options file, the server does no authentication of clients.
rlmadduser
is new in RLM v13.0. All components must be RLM v13.0 or
later for this functionality to work.