6.2.3.8 rlmreread - cause the license server(s) to reread their license and option file(s)
Usage: rlmreread [isv]
rlmreread
causes the specified ISV server isv
to reread it's license file, and options file if specified in the license file (or if in the default location isv.opt). If isv
is omitted, the reread command is sent to rlm and all ISV servers. If isv
is specified as rlm
, then only the rlm server rereads its license file.
When rlm
rereads its license file, it starts any new ISV servers that were not present before.
Note that rlm
performs an automatic reread of the license file(s) every night at midnight.
Note also that (on Unix systems only) the servers will do a reread if a SIGHUP signal is sent to the rlm
process.