6.2.7.1 How The ISV Options File is Located
The ISV options file can be located in 3 ways:
- You can specify the ISV options file location on the ISV line of The License File.
- If no specification is on the ISV line, RLM will look for <ISV>.opt (where <ISV> is the name of the ISV) in the location with the first license file.
- If there is no options file in either of the first 2 locations, RLM will look for <ISV>.opt in the working directory where you started the RLM server.