6.2.7.10 EXPRESS

EXPRESS [ON|OFF] <product>

The EXPRESS line controls queuing behavior for one or all products. If EXPRESS is turned on for a product, then queued requests which can be satisfied immediately are granted independent of whether other requests are ahead in the queue. If EXPRESS is turned off, then a queued request will always be placed at the end of the queue if it exists.

If the EXPRESS line does not specify a product, it applies to all products.

By default, EXPRESS is turned ON for all products in RLM.