6.2.7.23 REPORTLOG
REPORTLOG [+]file_path [std | small | detailed]
The REPORTLOG option instructs the ISV server to write a file suitable for usage reporting to the filename file_path. If file_path is preceded with a '+' sign, the new data is appended to the file, otherwise the file is overwritten.
The third (optional) argument specifies the format of the reportlog file. Valid values are:
- std - write the standard report log file (the default if this field is not present)
- small - a smaller report log file
- detailed - write a reportlog that logs check-in/checkout events down to the tenth of a millisecond
All reportlogs are authenticated.
If your server is writing a reportlog, it is important to shut the server down gracefully (i.e., don't kill the server, shut it down with the RLM web interface or with an rlmdown command, or via the service controller if running as a Windows service). If you don't do this, the sever won't write the final authentication record to the report log, and you will not be able to verify the last section of the report.
For details of the various output formats, 6.4.2 Reportlog File Format.
If a detailed reportlog is specified on Windows, RLM will produce a detailed reportlog, however, the fractional seconds field will always be 0.