6.2.7.14 INCLUDE

INCLUDE <product>
[user|host|group|host_group|internet|internet_group|project] <who> [id=nnn]

The INCLUDE line allows usage of a product by a particular user, host, group, host_group, IP address, or project. If you specify group, host_group, or internet_group, it must be defined by a GROUP or HOST_GROUP or INTERNET_GROUP line in the options file. Anyone not specified by the INCLUDE line is not allowed to use product.

INCLUDE has no effect on Named User licenses (the INCLUDE line will be ignored).

Portions of the INTERNET address can be specified with a '*' which matches any address, e.g., 172.16.7.*

Note that INTERNET and INTERNET_GROUP are ineffective on RLM Cloud servers where the application is using HTTPS transport.

If specified, the id applies this option to the license with an id of “nnn”.

Note: To use PROJECT the user needs to specify the project name in the environment variable RLM_PROJECT prior to starting the application. To use INTERNET, specify the internal (vs. external) IP address of the client machine.